"Generator has no Wi-Fi signal" message in Mobile Link

This message appears when your Mobile Link device cannot connect to your home Wi-Fi router. It may be caused by weak signal strength, a meshed network, router changes, or network outages. Mobile Link devices work on 2.4 GHz only, so a dedicated 2.4 GHz network or compatible extender may be needed. Troubleshooting steps include reconnecting the generator via the Mobile Link app, using a web browser, or redoing the initial setup. Customers searching for “generator won’t connect to Wi-Fi,” “weak Wi-Fi signal generator,” or “Mobile Link lost Wi-Fi” or "Generator has no Wi-Fi signal" will learn how to restore stable connectivity and reliable generator monitoring.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support