How do I test my generator in manual mode after clearing an error?

Clear a generator alarm or error code and run a no-load test in Manual mode to see if the same code returns. This procedure applies to air-cooled home standby generators with Power Zone 200, Evolution (Evo 1/Evo 2), Sync, and Nexus controllers. It explains safe no-load setup using the main line circuit breaker, how to start in MANUAL, what to do if the alarm comes back, and when to contact a dealer for intermittent generator errors and recurring alarms, helping restore safe, reliable operation.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support