What is the Load Shed Before Return to Utility Feature in Field Pro?

The “Load Shed Before Return to Utility” feature briefly pauses selected home appliances when utility power comes back after a generator outage. The generator momentarily lowers frequency to trigger Generac Energy Management devices to enter a load-shed state, helping the home switch back to utility power smoothly. Pauses typically last about 5 minutes, with an extra 15–30 seconds between multiple devices if several Energy Managers are installed. Installers enable this in the Field Pro app on the Generator Details → Configurations page by toggling the setting on. It’s best used to protect sensitive equipment—like air conditioners—when an immediate restart isn’t necessary.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support