Salesforce

What Error Codes Do I Need to Call a Dealer For?

« Go Back
Fields
What Error Codes Do I Need to Call a Dealer For?
What-Error-Codes-Do-I-Need-to-Call-a-Dealer-For
Content

Error Codes that Require an Authorized Service Dealer

Most error codes listed below exceed typical DIY troubleshooting and require a Generac Independent Authorized Service Dealer. Clearing simpler error codes can sometimes help determine if the issue persists. Users who wish to attempt clearing an alarm before contacting a dealer can follow instructions below or see How do I clear an error or alarm code on my standby generator? for more detail. A dealer can be located using the Generac Dealer Locator Tool.

Note: For a list of error codes that may be addressable by an end user, see: Where can I find a list of error codes for my generator?

Environment

These error codes apply to air and liquid cooled home standby generators. Error codes are displayed on the LCD display of the generator's controller. Note that not all generator controllers have an LCD screen. The generator's LED indicator light will be either yellow or red depending on the error.

Troubleshooting

Follow the below steps to determine if your error code requires service from a dealer:
 

1. Go to the front of the generator, lift the lid, and locate the Controller on the top right side of the generator.
2. Clear the alarm by pressing the red OFF button,  then the ENTER button.
Note: For the 7.5kW PowerPact unit press the OFF button twice to clear an active alarm or maintenance/warning. If an active alarm and maintenance/warning are present at the same time, press the OFF button 3 times to clear.
3. Attempt to start the generator in manual mode by pressing the Manual button.
Note: If the generator starts successfully in manual mode, it will continue to run until shut down with the AUTO or OFF button.
4. If the error code returns, dealer service is required: How Can I Find a Generac Service Dealer in My Area?

Error Codes

Error CodeDisplayed Alarm
134DTC
180, 1001Controller
1050VSCF Low Battery
1051VSCF High Battery
1058VSCF DC Under Voltage
1059VSCF Field Loss
1062VSCF Comms Loss
1063VSCF Enable Mismatch
1064VSCF Speed PWM Loss
1065Over Frequency
1500-1521RPM Sensor
1800 - 1803Overvoltage
1900 - 1916Undervoltage
2098, 2099Wiring Error
2399Stepper Overcurrent
2500-2502Bosch
2600 - 2602Ignition
2611 - 2620Over current cylinder 1 -10
2621 - 2630Under current cylinder 1-10
2650Internal Ignition Missing Cam
2651External Ignition Missing Cam
2660Internal Ignition Missing Crank Pulses
2661External Ignition Missing Crank Pulses
2671, 2672CAN Bus
2710Ruptured Tank
2790SEEPROM Abuse
2810Hall Calibration
2900 Diesel ECU Fault
2910Gaseous Emissions
3000, 3015Hardware Match Error
3001Speed Match Error
3002Fuel Match Error
3003ECM Initiated Emergency Shutdown
3100 - 3107, 3115, 3117Throttle Body Air
3200, 3215High Fuel Pressure
3201, 3217Low Fuel Pressure
3202 - 3204     Fuel Pressure
3300, 3315, 3317High Oil Pressure
3301Low Oil Pressure
3302 - 3304Oil Pressure
 3400, 3415High MAP
3401Low MAP
3402 - 3404MAP
3415High MAP
3417LCM MAP
3500, 3515High MAP Temp
3501, 3517LCM Map Temp
3502 - 3504MAP Temp
3600, 3601, 3615, 3617Check Air Filter
3602 - 3604Air Filter Sensor
3700, 3715High Coolant Temp
3701, 3717LCM Coolant Temp
3702 - 3704Coolant Temp 
 3803High Battery Voltage
3804LCM Battery Voltage
3900, 3915High Oil Temp
3901, 3917Low Oil Temp
3902 - 3904Oil Temp
4003, 4004Fuel System
 4100 - 4104Crankshaft Sensor
4200 - 4204Camshaft Sensor
4300 - 4304, 4315, 4317Check O2 Sensor
4400 - 4404, 4415, 4417 Engine Knock Sensor
4502 - 4507Ignition Coil 1
4602 - 4607Ignition Coil 2
4702 - 4707Ignition Coil 3
4802 - 4807Ignition Coil 4
4900 - 4907, 4915, 4917Fuel Mixer
5003, 5004CAC
5100, 5115RPM High
5101, 5117RPM Low
5102, 5107RPM

 


Powered by