Why won't my brand new generator battery stay charged?

Single-phase generators with the Nexus or Evolution control panel must have 120VAC input to the T1 terminal on the generator. This powers the controller's internal battery charger. If there is an issue with the T1 circuit, then the battery will not keep a charge. 

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support