Need help with Mobile Link? Visit the Mobile Link support site.

Pressure Washers

  • How Can I Find a Generac Service Dealer in My Area?

    This article explains how to find and contact a Generac Independent Authorized Service Dealer using the dealer locator, including how to select product categories, service options, and dealer designations. It also covers international dealer lookup, what to do if no nearby dealers appear, how warranty work is handled, and where to find...

  • What Type of Oil Should I Use in My Pressure Washer?

    This article explains which engine oil to use in a gas-powered pressure washer, including oil recommendations for the break-in period, temperature-based viscosity guidance, oil-change intervals, engine oil capacities, and specifications for selecting a high-quality replacement oil.

  • Troubleshooting Erratic Pressure, Loss of Pressure, and Low Water Volume in Pressure Washers

    Troubleshoot erratic pressure, loss of pressure, or low water volume on Generac pressure washers by checking water supply flow and hose condition, cleaning the inlet filter and nozzle, and verifying settings. The article also explains triplex pump callouts (A through F) and includes an updated procedure to purge air from the pump,...

  • Troubleshooting Pressure Washer Chemical/Detergent Injector Issues

    Common causes are the wrong nozzle is installed or the PowerDial setting is incorrect, the siphon hose filter is clogged, the detergent injector port is clogged, the siphon hose fitting is too loose, or the detergent mixture is too thick.

  • Troubleshooting Pressure Washer Water Leaks

    Water leaks typically occur at the pump, from the garden hose connection, or from connections between the pump and spray gun. Each of these failure points contains components that should be inspected for wear or improper connection.

  • Why won't my pressure washer start or stay running?

    A pressure washer may not start if it has a dirty air filter, old fuel, low fuel, a bad spark plug, a bad spark plug wire connection, or the choke is in the ON position.

No articles found
Loading