Need help with Mobile Link? Visit the Mobile Link support site.

Liquid-Cooled Standby Generators

  • Connect a generator to a home Wi-Fi network using a web browser (legacy method)

    Learn how to connect a Generac Guardian home standby generator with Mobile Link Onboard Wi-Fi, not the aftermarket Wi-Fi/Ethernet device or cellular accessory, to a 2.4 GHz network using a web browser when the Mobile Link app setup fails or the generator won’t connect to Wi-Fi. The steps show how to join the MLG network, open 192.168.51.1...

  • “Something has gone wrong”, “Something's wrong”, or "Status unknown"

    Explains what the “Something has gone wrong” and “Something's wrong” statuses mean and how to address them. Customers can identify their Wi-Fi or cellular connectivity device, verify hardware and network communication, reconnect the generator when needed, and determine when to contact a dealer or Mobile Link Support for reliable generator...

  • How do I activate my liquid-cooled generator with a Power Zone 410 controller?

    This article explains how to activate a liquid-cooled Generac standby generator equipped with the Power Zone 410 controller. It walks through opening the unit, preparing the controller, completing registration, connecting Wi-Fi, and setting the exercise schedule. These steps help customers who search for terms like generator activation,...

  • How Do I Activate My Home Standby Generator?

    This article explains how to activate Generac home standby generators, including Guardian series generators with Evolution controllers, 7.5 kW PowerPact models, and Next Generation Air-Cooled Standby Generators commissioned through the Field Pro app. It covers generator activation codes, warranty registration, Wi-Fi activation, first-time...

  • What Does It Mean When My Generator Displays an Error Code: Charger Missing AC, Code 2780?

    Explains Charger Missing AC code 2780, the T1 charging circuit conditions that can trigger it, and troubleshooting for Guardian and Next Generation home standby generators. It also explains when some Next Generation generators may continue showing the warning even though the battery is charging normally and when an IASD should perform...

  • What Error Codes Do I Need to Call a Dealer For?

    This article helps owners identify error codes, alarms, and warnings on Generac air-cooled home standby generators. It explains which Next Generation and Guardian Series codes may require dealer service, how to clear an alarm, and where to find dedicated troubleshooting articles for specific codes so customers can take the right next...

  • How does cold weather impact Home Standby fuel systems?

    Explains how cold weather can affect liquid propane (LP) and natural gas fuel systems for home standby generators. It describes how reduced propane tank pressure can affect vaporization, why exact cold-weather limits depend on the supplied fuel, and when customers should contact their fuel supplier to support reliable generator operation.

  • Do Generac Home Standby Generators have cold weather accessories or Cold Weather Kits?

    Learn which cold weather accessories are available for Guardian, Next Generation Series, PowerPact, and liquid-cooled home standby generators. This article explains battery pad warmers, wrap-around battery warmers, oil filter warmers, and breather warmers, including temperature guidance, compatibility, and part numbers for reliable...

  • What Does It Mean When My Generator Displays an Alarm: Low Oil Pressure, Error Code 1300?

    When your home standby is displaying an Error Code: Low Oil Pressure, Code 1300, the first thing to check is your oil level.  If oil is needed, add oil per recommendations in your owner’s manual.  Be careful not to overfill the engine.  If the oil level is good and your unit is still not working, a service call is needed.

No articles found
Loading