Need help with Mobile Link? Visit the Mobile Link support site.

Troubleshooting

  • How do I hard reset or power cycle a Mobile Link device?

    Explains when a hard reset or power cycle may be necessary to resolve Mobile Link connectivity issues on Generac home standby generators. Includes device-specific reset and reconnection instructions for Next Generation, Guardian Series, and liquid-cooled generators, along with guidance for checking whether communication has been restored.

  • Generator has No LTE Signal

    Learn what a “generator has no LTE signal” status means in the Mobile Link and ecobee by Generac apps and how to troubleshoot the generator’s cellular connection. The steps cover the current Connectivity Cellular Accessory and discontinued 4G LTE accessory, including antenna checks, LED status guidance, and possible local carrier outages,...

  • No Network Connection Error when accessing the Mobile Link App

    The No Network Connection message appears when the app has been opened and cannot detect a network connection on the phone after approximately 8 seconds. The message indicates that the phone does not currently have a network connection that the app can use.

  • Troubleshooting home standby generator setup in the ecobee by Generac app

    Use this article when a home standby generator does not appear, shows offline, or displays a different status in the ecobee by Generac app. It covers Mobile Link enrollment, matching account information, app updates, the one-generator-per-home limitation, and features that still need to be managed through Mobile Link.

  • What Does It Mean When My Generator Displays an Error Code: Charger Missing AC, Code 2780?

    Explains Charger Missing AC code 2780, the T1 charging circuit conditions that can trigger it, and troubleshooting for Guardian and Next Generation home standby generators. It also explains when some Next Generation generators may continue showing the warning even though the battery is charging normally and when an IASD should perform...

  • What Error Codes Do I Need to Call a Dealer For?

    This article helps owners identify error codes, alarms, and warnings on Generac air-cooled home standby generators. It explains which Next Generation and Guardian Series codes may require dealer service, how to clear an alarm, and where to find dedicated troubleshooting articles for specific codes so customers can take the right next...

  • Why Won't My Generac Portable Generator Produce Power?

    Provides general troubleshooting for Generac portable generators that start and run but do not supply power to connected appliances or tools. It walks customers through checking loads, breakers, GFCI receptacles, cords, and model-specific resets before determining whether additional service is required.

  • Why is my portable generator's carburetor leaking fuel when I turn on the fuel valve?

    Explains how to troubleshoot fuel leaking from a portable generator carburetor, including a loose drain screw or stuck float needle. It also explains how to check for continued leaks and prevent future carburetor problems, helping customers troubleshoot safely and maintain reliable generator operation.

No articles found
Loading