Need help with Mobile Link? Visit the Mobile Link support site.

  • Generator has No LTE Signal

    Learn what a “generator has no LTE signal” status means in the Mobile Link and ecobee by Generac apps and how to troubleshoot the generator’s cellular connection. The steps cover the current Connectivity Cellular Accessory and discontinued 4G LTE accessory, including antenna checks, LED status guidance, and possible local carrier outages,...

  • Do Generac Home Standby Generators have cold weather accessories or Cold Weather Kits?

    Learn which cold weather accessories are available for Guardian, Next Generation Series, PowerPact, and liquid-cooled home standby generators. This article explains battery pad warmers, wrap-around battery warmers, oil filter warmers, and breather warmers, including temperature guidance, compatibility, and part numbers for reliable...

  • Is my Wi-Fi network compatible with Mobile Link's Onboard Wi-Fi Module?

    This article explains Wi-Fi compatibility for Generac home standby generators using Mobile Link. Generators with onboard Wi-Fi or Wi-Fi/Ethernet devices must connect to a dedicated 2.4 GHz network, since 5 GHz is not supported. Customers searching for “generator Wi-Fi compatibility,” “generator won’t connect to Wi-Fi,” or “weak Wi-Fi...

  • How Can I Contact Mobile Link Customer Support?

    This article explains how Mobile Link customers can contact support by email, phone in the United States or Canada, or through the Mobile Link app. It also directs customers to the Generac Product Assistant and Mobile Link troubleshooting resources for common questions, helping them find answers quickly or connect with the Mobile Link...

  • How Do I Contact Generac Customer Support?

    Generac's customer support can be contacted via phone, chat, and email on Generac.com: https://www.generac.com/service-support/contact-us

  • How do I connect my generator to a home Wi-Fi network?

    A Wi-Fi connection can be established using the Mobile Link for Generators Android or iPhone application. Alternatively, the connection can be established by accessing the generator's MLG network through a browser on a PC or mobile device.

  • How do I set up Wi-Fi as a backup for my Connectivity Cellular Accessory?

    This article explains how to configure or remove Wi-Fi backup for the Connectivity Cellular Accessory device using the Mobile Link or Field Pro app. It covers Bluetooth requirements, staying near the generator, troubleshooting connection problems, and removing Wi-Fi backup when needed to help reduce the risk of missed Mobile Link...

No articles found
Loading