Need help with Mobile Link? Visit the Mobile Link support site.

Product Accessories

  • Do Generac Home Standby Generators have cold weather accessories or Cold Weather Kits?

    Learn which cold weather accessories are available for Guardian, Next Generation Series, PowerPact, and liquid-cooled home standby generators. This article explains battery pad warmers, wrap-around battery warmers, oil filter warmers, and breather warmers, including temperature guidance, compatibility, and part numbers for reliable...

  • What surfaces can I install my home standby generator on?

    The article explains the three approved surfaces for preparing a mounting surface for air-cooled home standby generators: compacted, leveled pea gravel or crushed stone, approved composite pad and approved concrete base pad. It is important to follow national, state, or local building codes when dealing with installing the generator, and...

  • Generac Load Manager Troubleshooting Guide

    This article provides a guide to troubleshooting basic issues with Generac Load Managers (formerly known as smart management modules SMM)

  • How to set priorities for Generac Load Manager

    This guide outlines how to set priorities and ensure that high-priority loads recover first during generator overloads or power outages. It covers assigning priority levels, applying a priority decal to the electrical panel, and recording the priorities for future reference.

  • What is a Soft Starter?

    A soft starter is an electrical device used with alternating current motors to reduce the electrical load demand on the generator when energy-intensive devices start. This reduction is achieved through reducing the startup current of the appliance's motor and reducing the torque to improve efficiency. SureStart Soft Starter is compatible...

  • What is a Power Management Module (PMM)?

    The Power Management Modules (PMMs) is a 50A, 24VAC rated contactor. Through the use of PMMs, up to 4 large electrical loads can be managed when used in conjunction with some 100-800A, single-phase switches utilizing an Overload Prevention Control Board (OPCB). This allows for the use of a smaller, more affordable generator system.

  • Setting the lockout switch on Generac Load Manager

    This guide outlines how to set the lockout switch on the Load Manager. It covers lockout switch positions, how they are related to Utility or Generator Mode, and the functions of those modes and lockout switch positions.

No articles found
Loading