Need help with Mobile Link? Visit the Mobile Link support site.

Mobile Link Wi-Fi & Ethernet Device

  • How do I hard reset or power cycle a Mobile Link device?

    Explains when a hard reset or power cycle may be necessary to resolve Mobile Link connectivity issues on Generac home standby generators. Includes device-specific reset and reconnection instructions for Next Generation, Guardian Series, and liquid-cooled generators, along with guidance for checking whether communication has been restored.

  • What are the available Mobile Link subscription plans?

    Mobile Link offers Basic and Premium monitoring plans for compatible Generac generators and fuel monitors. Compare subscription features, pricing, device limits, supported controllers, and renewal options to choose the appropriate monitoring plan. Learn how hardware compatibility and subscription level affect available functionality so...

  • Is my Wi-Fi network compatible with Mobile Link's Onboard Wi-Fi Module?

    This article explains Wi-Fi compatibility for Generac home standby generators using Mobile Link. Generators with onboard Wi-Fi or Wi-Fi/Ethernet devices must connect to a dedicated 2.4 GHz network, since 5 GHz is not supported. Customers searching for “generator Wi-Fi compatibility,” “generator won’t connect to Wi-Fi,” or “weak Wi-Fi...

  • How Can I Contact Mobile Link Customer Support?

    This article explains how Mobile Link customers can contact support by email, phone in the United States or Canada, or through the Mobile Link app. It also directs customers to the Generac Product Assistant and Mobile Link troubleshooting resources for common questions, helping them find answers quickly or connect with the Mobile Link...

  • How do I connect my generator to a home Wi-Fi network?

    A Wi-Fi connection can be established using the Mobile Link for Generators Android or iPhone application. Alternatively, the connection can be established by accessing the generator's MLG network through a browser on a PC or mobile device.

No articles found
Loading