Read the owner's manual thoroughly to understand all of the instructions, cautions, and warnings before using this equipment. If any section of the manual is not understood, contact your nearest authorized dealer, or contact Generac Customer Service at 1-888-436-3722 (1-888-GENERAC), or www.generac.com with any questions or concerns.
Auto mode for home standby generators
Generac home standby generators can operate in MANUAL or AUTO mode. When the generator is placed in AUTO mode, the controller monitors utility power and allows the generator to operate automatically when needed.
When a properly installed and operational home standby generator is in AUTO mode, the system can:
- Automatically start the generator when a qualifying utility power outage is detected.
- Signal the automatic transfer switch to transfer connected electrical loads to generator power when the appropriate operating conditions are met.
- Signal the transfer switch to return connected loads to utility power after acceptable utility power has been restored.
- Complete the normal shutdown or cooldown sequence after utility power is restored, as applicable to the generator model.
To place a generator in automatic mode, press the AUTO button on the generator control panel. The location of the button and the method for verifying AUTO mode vary by controller type. Follow the applicable instructions below.
IMPORTANT: If the generator has recently undergone maintenance or is being returned to service during a utility outage, additional checks may be necessary before selecting AUTO. Follow the applicable safety instructions and see How do I return a generator to automatic mode after service?
IMPORTANT: For a newly installed home standby generator, verify that all required electrical checks, installation procedures, and initial startup requirements have been completed according to the installation manual before placing the generator in AUTO mode. Incomplete installation or improper electrical connections could result in equipment damage or personal injury. Generac strongly recommends that installation and initial startup be performed by an Independent Authorized Service Dealer.
Note: A generator must be activated before normal operation in AUTO mode. For more information, see How do I activate my home standby generator?

Environment
This article applies to Generac residential home standby generators equipped with the following control panels:
Select the appropriate controller above to learn more about its features and operation. The instructions below are organized by controller type.
This article includes
Power Zone 200 control panel
Follow these instructions for compatible Next Generation air-cooled home standby generators equipped with a Power Zone 200 controller.
- Go to the generator and unlock the lid.
- Open the lid and locate the control panel on the right side of the generator.
- Press the AUTO button.
- Verify that the generator is in AUTO mode by checking for the green status indicator LED on the right side of the generator.
Note: If the green status indicator is not illuminated, or a red, yellow/orange, or blue indicator is displayed, additional attention may be required. See What do the green, yellow, blue, and red status indicator lights mean on home standby generators?

What if I cannot put the generator in AUTO mode?
Check whether the generator is in SERVICE mode, indicated by a blue LED on the control panel. For more information, see Why can't I put my generator into automatic mode?
Evolution control panel
Follow these instructions for home standby generators equipped with an Evolution control panel.
- Go to the generator, unlock the lid, and raise the cover.
- Locate the control panel on the right side of the open generator. The display may show SWITCHED TO OFF. Press the AUTO button.

- Verify that the generator returns to the READY TO RUN screen, indicating that the controller is in automatic mode and ready for normal operation.

Power Zone 410 control panel
Follow these instructions for compatible residential liquid-cooled home standby generators equipped with a Power Zone 410 controller.

- Access the generator control panel.
- Verify that the Generator Emergency Shutdown switch (H) is set to the CLOSED (ON) position.

- If an active alarm is present, identify and address the underlying condition before clearing the alarm. When appropriate, navigate to the Alarm Screen and press OFF, then ENTER, to clear the alarm. For additional information, see How do I clear an error or alarm code on my home standby generator?
- Press the AUTO button (A).
- Press ESCAPE (E) to return to the main menu. The date and time should appear at the top of the screen.

- Confirm that the display shows Status: Ready to Run.
IMPORTANT: Do not repeatedly clear an active alarm without identifying and correcting its cause. If an alarm returns or the generator cannot be placed in AUTO mode, contact an Independent Authorized Service Dealer for assistance.
For more information about the controller interface and navigation, see the Power Zone 410 menu map.
Troubleshooting
Generator status is not updating in Mobile Link
After changing the generator to AUTO mode, the updated status may not appear immediately in Mobile Link. The generator control panel displays the local operating status and should be checked first to confirm the selected mode.
If the status does not update in Mobile Link after allowing time for communication, a connectivity issue may be preventing the information from reaching the app. See Why doesn't Mobile Link display the correct generator status?
Generator does not start during a utility outage
When operating normally in AUTO mode, a home standby generator is designed to start automatically after detecting a qualifying loss of utility power. However, an active alarm, an incomplete installation or activation, or another condition preventing operation may stop the generator from starting.
Verify the generator's current status using the control panel. If an alarm or fault condition is present, follow the applicable instructions in the owner's manual. Contact an Independent Authorized Service Dealer if the generator does not start and the cause is unclear.
Generator starts even though utility power is available
A generator operating in AUTO mode may start for reasons other than a utility outage, including scheduled exercise cycles. For more information, see Why would my home standby generator start running when my home still has utility power?
Generator cannot be placed in AUTO mode
If the generator does not enter AUTO mode, check the following:
- Activation: Verify that the generator has completed the required activation process. See How do I activate my home standby generator?
- Service mode: Check whether the generator is in SERVICE mode. For applicable controllers, a blue status light may indicate Service mode. See Why can't I put my generator into automatic mode?
- Active alarms: Review any active alarm or fault messages and follow the troubleshooting instructions in the owner's manual. Do not clear recurring alarms without correcting their underlying cause.
If the generator still cannot be placed in AUTO mode, contact an Independent Authorized Service Dealer for additional assistance.