Need help with Mobile Link? Visit the Mobile Link support site.

Manual Transfer Switches

  • What is the layout of the control wires and what do they do?

    In a Generac Home Standby Generator installation, control wires play an essential role in allowing proper communication between the generator, transfer switch, and utility power source. The N1/N2, T1, 23/194, and 0/DC Common wires are key control wires that must be properly connected for optimal performance, and regular maintenance checks...

  • Why doesn’t every Generac home standby generator come with a required transfer switch?

    Generac home standby generators do not always include a transfer switch because each home requires a different switch type and size based on factors like electrical service, how much of the home needs backup power, local code requirements, and load‑management needs. Selling generators and transfer switches separately ensures customers get...

  • What is an interlock kit?

    An interlock kit is a mechanical safety device that prevents a home’s main breaker and a generator breaker from being ON simultaneously. It provides a cost-effective, code-compliant way to power essential circuits from a generator during outages. While simpler and less expensive than a manual transfer switch, interlock kits offer less...

  • What Is the Difference between a NEMA 1 and NEMA 3R Rated Transfer Switch?

    The main difference between a NEMA 1 and NEMA 3R rated transfer switch is the level of protection they provide against environmental conditions. A NEMA 1 rated transfer switch is intended for indoor use and offers basic protection against dust, falling dirt, and dripping water. In contrast, a NEMA 3R rated transfer switch is intended for...

  • What Are the N1 and N2 Control Wires Responsible For?

    The N1 and N2 control wires are responsible for detecting any loss or restoration of utility power. In case of a voltage drop on these connections, the generator will automatically start to provide power backup.

  • What is a Manual Transfer Switch?

    A manual transfer switch (MTS) is a safe way to connect a portable generator to a home, preventing dangerous backfeeding or back feeding into utility lines and allowing users to manage loads without overloading the generator. An MTS requires a Power Inlet Box (PIB) and works only with certain portable generators, not automatic standby...

  • Where can I find information about the cost of a transfer switch?

    Explains transfer switch pricing and what affects cost including size, voltage, and enclosure type. Notes that installation is separate. Includes how to view MSRP on Generac.com and when to schedule an in-home consultation. Search: switch cost, transfer switch price, install cost, MSRP.

  • Where Is My Serial Number Located on My Transfer Switch?

    To find the serial number of your Generac Transfer Switch, check various locations depending on the model, but generally, it is printed on a data label that can be found inside the switch, either on the top of the back panel or on the upper or lower sections of the inside-left panel.

  • Why you should never back-feed your electric panel with a generator

    This article explains backfeeding, also spelled back-feeding or back feed, a dangerous condition where electricity from a portable generator flows in reverse into utility lines, creating risks of electrocution, fire, and equipment damage, and violating electrical codes. It describes how improper generator connections, such as using a...

No articles found
Loading