What is the layout of the control wires and what do they do?
In a Generac Home Standby Generator installation, control wires play an essential role in allowing proper communication between the generator, transfer switch, and utility power source. The N1/N2, T1, 23/194, and 0/DC Common wires are key control wires that must be properly connected for optimal performance, and regular maintenance checks...