Need help with Mobile Link? Visit the Mobile Link support site.

Power Stations

  • GB Power Station and solar panel compatibility

    This article explains how to connect Generac solar panels to compatible Generac GB power stations. It covers GB Power Station and solar panel compatibility, setup order, solar panel positioning, same-model panel requirements, solar input limits, and safe disconnection.

  • How do I charge my GB power station?

    This article explains how to charge the GB1800 power station using AC wall charging, Generac solar panels, car charging, and simultaneous AC and DC input. It also describes Eco, Standard, and Boost charge modes, supported charge temperatures, and charge time expectations.

  • Why won’t my GB power station charge?

    This article helps troubleshoot a GB power station that will not charge from AC power, solar panels, or a vehicle 12 V source. It covers source compatibility, loose connections, temperature limits, AC circuit breaker reset, solar input limits, and car charging precautions.

  • How long will my power station run?

    This article explains how to estimate GB power station runtime using watt-hours, device wattage, and the runtime formula from the owner’s manual. It includes common runtime examples and explains why actual runtime may vary based on load, surge power, temperature, and device behavior.

  • What is a GB power station?

    This article explains what a Generac GB power station is and answers common battery questions for GB Series portable power stations, including whether the integrated lithium battery can be replaced, how long the battery lasts, how to charge the unit, and where to get service. It helps customers compare power stations with portable...

  • What do the fault lights on my GB series power station mean?

    This article provides a comprehensive guide on the fault lights of Generac GB Series Portable Power Stations, discussing the various warnings such as fault, low temperature, high temperature, and flashing AC/DC, along with their meanings and resolutions for operating issues. Users are guided on how to address solid and flashing fault...

  • How Long Does It Take To Recharge the GB Series Portable Power Stations?

    Using the built-in AC charging adapter that is included with the unit, the GB1000 - 0-80% recharge time is about 2.1 hours. The GB2000 - 0-80% recharge time is about 4 hours. Fast-charging accessories are available (Model Numbers: 8031 and 8030) which can improve charge speeds. 

No articles found
Loading
11 Articles