Salesforce

How do I replace the battery on my home standby generator?

« Go Back
Fields
How do I replace the battery on my home standby generator?
How-do-I-replace-the-battery-on-my-home-standby-generator
Content

Read the manual thoroughly and understand all of the instructions, cautions, and warnings before using this equipment. If any section of the manual is not understood, contact your nearest authorized dealer, or contact Generac Customer Service at 1-888-436-3722 (1-888-GENERAC), or www.generac.com with any questions or concerns. 

Replacing the generator's battery

Generator owners should reference these articles before performing maintenance on the generator:

Environment

This article applies to Generac air-cooled home standby generators.

If you have a Next Generation series generator, see here.
 
If you have a Guardian series generator, see here.         
  
        

Before you begin

Verify the correct battery will be installed. See What Battery Do I Need for My Home Standby Generator? for information about compatible batteries.

Verify the battery requires replacement. Reference How Do I Inspect the Battery On My Home Standby Generator? for steps to inspect and service the current battery.

Guardian series generators: video instructions

To replace the generator's battery

1. Lift the generator's lid and set the generator main line circuit breaker (MLCB) to off.

2. Press the OFF button on the generator control panel. This will prevent the generator from starting in the following step.

3. Set the utility main line circuit breaker (MLCB) to off. See What is a service entrance disconnect and how can I tell if it's on or off? for more information.

Note: Setting the utility main line circuit breaker (MLCB) to off will shut off the utility power to the home until the utility MLCB is restored to the on position.


4. If running during an outage, allow the generator to run and cool down for five minutes with no load applied.

Note: Setting the generator main line circuit breaker (MLCB) to off removes the load from the generator. Failure to remove the load and cool down before shutting the generator off can cause damage.


5. Press the OFF button to power off the generator. Then remove the front panel. See How do I remove the front panel on my home standby generator? for steps to remove the front panel.

6. Allow the generator to cool for an additional five minutes before working on it.

7. Remove the 7.5A fuse from the generator's control panel to prevent the battery from draining. This is located underneath the rubber flap (B) shown in Figure 1-1.

image.png
Figure 1-1

8. Remove the intake side panel. See How Do I Remove the Generator Side Panel? for more information.

9. Disconnect the white battery charger cable located beneath the control panel, shown in Figure 1-2.

image.png
Figure 1-2

10. Be sure the wrench never makes contact with both posts at the same time. This will cause a short and can be very dangerous. Disconnect the battery, removing the negative battery cable first and then the positive cable.

11. Remove the disconnected battery and insert the new battery.

12. Connect the positive battery cable first and then the negative battery cable.

13. Tighten the battery cable lugs with a wrench. Again, avoid damage and injury by preventing the wrench from making contact with both battery posts at the same time.

14. Reconnect the battery charger cable.

15. Reinstall the intake side panel and the front panel.

16. Reinstall the 7.5A fuse.

17. When the control panel boots up, the install wizard should appear.

18. This will allow you to set the current time and date (military time).

19. Set the generator's main line circuit breaker to ON.

20. Set the utility main line circuit breaker to ON, restoring utility power to your house.

21. Place the generator in auto mode.

22. The generator is now ready to run in the event of a power outage.

23. Close the generator lid.

Battery Disposal 

Always recycle batteries in accordance with local laws and regulations. Contact your local solid waste collection site or recycling facility to obtain information on local recycling processes. For more information on battery recycling, visit the Call2Recycle website.

Next Generation series generators

1. Lift the generator's lid and set the generator main line circuit breaker (MLCB) to off.

2. Press the OFF button on the generator control panel. This will prevent the generator from starting in the following step.

3. Set the utility main line circuit breaker (MLCB) to off. See What is a service entrance disconnect and how can I tell if it's on or off? for more information.

Note: Setting the utility main line circuit breaker (MLCB) to off will shut off the utility power to the home until the utility MLCB is restored to the on position.

4. If running during an outage, allow the generator to run and cool down for five minutes with no load applied.

Note: Setting the generator main line circuit breaker (MLCB) to off removes the load from the generator. Failure to remove the load and cool down before shutting the generator off can cause damage.

5. Verify generator is in OFF mode, then lift the lid and remove the front panel: How do I remove the front panel on my home standby generator?

6. Remove the 7.5A fuse from control panel. 

7. Remove the intake side panel: How Do I Remove the Generator Side Panel?

8. Remove the controller top cover. 

9. See Figure 4-7. Disconnect J6 (2 wire connector) at the controller to disconnect battery charger AC input T1/Neutral cable.
 


10. Disconnect battery cables, removing the black negative battery cable first. 

11. Remove the old battery from battery tray and place the new battery in battery tray.

12. Connect the battery cables correctly. Damage will occur if battery is connected incorrectly.
a. Connect red positive battery cable to positive battery terminal. Tighten to 45- 50 in-lbs. (5-6 Nm).
b. Connect black negative battery cable to negative battery terminal. Tighten to 45- 50 in-lbs. (5-6 Nm). 
c. Install red battery terminal cover on red positive terminal. 

13. Connect J6 (2 wire connector) at the controller to connect battery charger AC input T1/Neutral cable.

14. Install controller top cover and intake side panel.

15. Insert 7.5A fuse into generator control panel.

16. Press AUTO button on controller.

17. Install front panel and close generator lid.

Battery Disposal

Always recycle batteries in accordance with local laws and regulations. Contact your local solid waste collection site or recycling facility to obtain information on local recycling processes. For more information on battery recycling, visit the Call2Recycle website.


Powered by