Need help with Mobile Link? Visit the Mobile Link support site.

Outage Content

  • How do I manually operate an automatic transfer switch?

    The article explains the difference between service-entrance rated and non-service-entrance rated transfer switches and warns against opening switches without an inner dead front cover. It provides instructions on how to operate a manual transfer switch and emphasizes caution due to potential electrocution or equipment damage....

  • Why Didn't My Home Standby Generator Turn On During a Power Outage?

    Use this article if your Generac home standby generator does not start when utility power is lost. It covers what to check on the control panel or Mobile Link, including Auto mode, alarms, and common power and battery-related causes. If internet is down and Mobile Link is unavailable, it also links to instructions for running the...

  • How do I prepare my portable generator for a storm?

    This article provides guidelines for preparing, operating, and managing portable generators during a storm to provide backup power during outages. It covers aspects such as inspecting, maintaining, placement, starting operation, monitoring operation, electrical safety, periodic shutdowns, refueling safety, and shutting down the generator...

  • Troubleshooting guide for home standby Generators during an outage

    Troubleshooting steps for air-cooled home standby generators during a utility outage, including: generator won’t start, or the generator is running but the home has no power (no power, not supplying power, running but no electricity, generator on but house/off, gen is running i dont have power, outlets dead, not transferring, transfer...

  • Is it safe to run my home backup generator after a storm surge or hurricane?

    This article explains how to safely inspect and operate a home standby generator after a storm surge or flooding event. It outlines what to do if the generator has been exposed to water, emphasizing that the unit must never run while submerged or surrounded by standing water. Customers learn when to contact an Authorized Service Dealer,...

  • What steps do I need to take to maintain my home standby generator after an extended outage?

    The article provides guidance for Generac home standby generator owners to identify and perform maintenance after extended outages. Owners can use the Mobile Link to check the previous maintenance schedule, log the run hours when maintenance was last performed, and then compare with the current generator run hours to identify required...

  • How to temporarily disable my generator?

    This article explains how to temporarily disable a Generac home standby generator system in emergency situations or when leaving a home for an extended period of time to prevent damage due to continuous use for over 24 hours. There are different shut down procedures depending on the presence of utility power and the operating status of...

No articles found
Loading