What Does It Mean When My Generator Displays an Alarm: Low Oil Pressure, Error Code 1300?

When your home standby is displaying an Error Code: Low Oil Pressure, Code 1300, the first thing to check is your oil level.  If oil is needed, add oil per recommendations in your owner’s manual.  Be careful not to overfill the engine.  If the oil level is good and your unit is still not working, a service call is needed.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support