What does it mean when my generator displays an alarm: Charger Warning, Error Code 2770
Error code 2770, labeled "CHARGER WARNING," indicates that the battery is not charging properly due to a blown T1 fuse or an issue with the charging circuit. Basic troubleshooting includes checking the battery health, verifying charging connections, and ensuring there is no corrosion at the battery terminals. If problems persist, it is...