What Does It Mean When My Generator Displays an alarm: RPM Sensor Loss, error codes 1500-1521?

To restart a generator that has shut down with an RPM Sense Loss alarm, first clear the alarm and then try restarting it. If it still does not start, remove some of the loads and try again or contact an authorized service dealer. If the generator will not start in AUTO when there is a utility loss due to an RPM Sense loss alarm, try checking the battery and battery cables, replace the battery if needed or contact an authorized service dealer.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support