Need help with Mobile Link? Visit the Mobile Link support site.

Field Pro

  • What does access denied or invalid security token mean in Field Pro?

    Provides troubleshooting instructions for the "Access Denied - You do not have a valid security token" error when connecting to a home standby generator through Field Pro. Covers internet connectivity, app version 1.14.2 or later, generator serial number verification, signing out and back in, reinstalling the app, and preparing for...

  • Serial number displays as "FFFFFFFFFF" in Field Pro

    This article explains what to do when the Field Pro app displays FFFFFFFFFF instead of a generator's serial number. It provides separate support guidance for Independent Authorized Service Dealers and non-authorized installers or other users so they can contact the appropriate resource for assistance.

  • How Do I Commission a Generator in the Field Pro Application?

    Explains how installers commission generators with a Power Zone 200 controller using the Field Pro mobile app, including the required on-site Bluetooth connection, registration, configuration, system testing, and activation. It also explains Mobile Link date and time behavior and optional ATS registration to help ensure the generator is...

  • How do I set up Wi-Fi as a backup for my Connectivity Cellular Accessory?

    This article explains how to configure or remove Wi-Fi backup for the Connectivity Cellular Accessory device using the Mobile Link or Field Pro app. It covers Bluetooth requirements, staying near the generator, troubleshooting connection problems, and removing Wi-Fi backup when needed to help reduce the risk of missed Mobile Link...

  • How do I fix the “Connected to another mobile device” message in the Field Pro app?

    Fix the Field Pro message “Connected to another mobile device” when connecting to a Next Generation air-cooled standby generator with a PowerZone 200 control panel. This article explains why it happens and how to resolve it by ensuring only one device is connected, power-cycling the connectivity module, and reinstalling Field Pro, so you...

  • Why does Field Pro indicate 'Firmware Update In Progress' when connecting to the generator?

    Learn how to view your generator firmware versions in the Field Pro app for Next Generation generators with the PowerZone 200 controller. This article explains how firmware updates happen through over-the-air FOTA when Wi-Fi or cellular is available, what to do if a firmware update is in progress too long, and what can block updates such...

  • How to use Field Pro in an offline environment

    This article explains how to prepare a Next Generation Series home standby generator for offline access using the Generac Field Pro app before a site visit with no Wi-Fi or cellular service. It walks through selecting “Prepare for a Future Visit,” finding and registering the generator if needed, and confirming the offline access window,...

  • Field Pro product registration says "We couldn't verify this address"

    If Product Registration shows “We couldn’t verify this address,” the address validation service may not recognize the address yet, such as in new development areas. Contact Generac Customer Support at 1-888-922-8482 to complete registration, then use Recheck registration status to confirm, for reliable registration status in the app.

  • Troubleshooting Bluetooth connection issues in the Field Pro app

    This article provides troubleshooting steps for resolving Bluetooth connectivity issues between the FieldPro app and generators equipped with a PowerZone 200 controller. It includes checks for battery connection, proximity to the generator, LED status indicators, and proper cable connections.

No articles found
Loading